iTHERM TrustSens receives readers’ award

Self-calibrating thermometer recognized as part of the 2019 Control Engineering Engineers’ Choice Awards

2019 kicks-off with good news. The iTHERM TrustSens self-calibrating thermometer received the 2019 Engineers’ Choice Award from US industry publication Control Engineering. The Endress+Hauser innovation took the top spot in the Process Control/Process Sensors category based on a reader’s poll. The Field Xpert SMT70 was also recognized, receiving honorable mention in the Industrial Tablets category.

The iTHERM TrustSens thermometer was designed specifically for hygienic and aseptic applications in the food & beverage and life sciences industries. TrustSens in-situ, automated and fully traceable self-calibration eliminates the risk of non-conformities, leading to superior product safety and process efficiency. The integrated Heartbeat Technology enables continuous self-diagnostics and verification without process interruption. The fully traceable calibration complies with GMP guidelines.

Mobile plant asset management with the Field Xpert SMT70

The robust Field Xpert SMT70 tablet PC allows plant operators to manage field instruments with digital communication interfaces in hazardous and non-hazardous areas. Access to field devices, also from third-party manufacturers, and the interface to the new digital service "Library" enables an efficient and modern instrument management.

The easy-to-use Field Xpert SMT70 with touch interface provides a pre-installed device driver library and supports HART, PROFIBUS DP/PA, FOUNDATION Fieldbus, Modbus and all Endress+Hauser service protocols.

Engineers’ Choice Award

The Engineers’ Choice Awards are handed out by US industry publication Control Engineering. In total, there were 26 categories readers were able to vote for their favorite product. The evaluation criteria included technological advancement, service to the industry, and market impact. An awards ceremony will be held on 8 April 2019 in Chicago, Illinois.

The 2019 Engineers’ Choice Award is the eighth time that the iTHERM TrustSens has been recognized ©Endress+Hauser

Product innovation: The 2019 Engineers’ Choice Award is the eighth time that the iTHERM TrustSens has been recognized since it was introduced to the market.

The Field Xpert SMT70 industrial tablet provides plant operators modern plant asset management ©Endress+Hauser

The Field Xpert SMT70 industrial tablet provides plant operators modern plant asset management in hazardous areas as well.

Contato